Other Parts Discussed in Thread: PCM5122, PCM5102
Hi,
Can PCM5102A be used for Non-Audio application with sampling frequencies 12.8KHz, 180KHz and 256KHz? Is PCM5102A is dedicated for only common audio frequencies listed in datasheet(8 kHz, 16 kHz, (32 kHz - 44.1 kHz - 48 kHz), (88.2kHz - 96kHz), (176.4 kHz - 192 kHz), and 384KHz)?
In the datasheet, Table 10 listed only 10 common audio sampling frequencies. If I want to use PCM5102A for some other frequencies which is not mentioned in Table 10, How can I implement that?
I am interfacing this DAC as slave and FPGA as master. So any PLL configuration can be done for Non-specified sampling frequency?