Part Number: TPA3110D2
No audio output from TPA3110D2.
Hello TI,
I'm making a circuit using TPA3110D2, in PBTL configuration.
I saw that is necessary to keep the pin SD at least 2V to keep it in HIGH position, but using the 100K resistor that is showed in the datasheet only gives 0,8V. Then I cheked and there are only 2K from SD to GND, then giving 2V to SD needs a very low resistence, and also lot of power, wich probably could break the IC.
In the datasheet shows that in PBLT configuration, it only gives audio only to one of the 4 inputs, I tried with one and with the 4 inputs connected, but I don't get any output.
I share my schematics, and hope anyone knows what's wrong. I hope it's something not really important,
Thank you.
Adrian.