Other Parts Discussed in Thread: TLV320AIC3104-Q1, TAS5431-Q1, TPD3S714-Q1
Dear Team,
Could you help to check does TAS5411-Q1 can meet spec as below?
Speaker interface: The emergency call module requires a built-in audio amplifier circuit to drive (power supply: 4W, 4Ω) a dedicated speaker for the emergency call system. When an E-call occurs, the emergency call module directly drives the dedicated speaker to sound; the emergency call module is for a dedicated speaker The speaker has self-diagnosis function; -->It's ok. Choose TAS5411-Q1
Dual microphone interface
1. MIC IN: The emergency call module can support 1 MIC IN power supply (whoever uses it supplies power), supports 1 MIC IN signal input, and under certain circumstances, can BY BASS two MIC signals to the HU; emergency call module Powers 1 microphone (8V, 10mA)); the emergency call module provides self-diagnosis function for the microphone;
2. MIC OUT: HU provides 1 MIC IN interface to the emergency call module. When the MIC is connected to the emergency call module, the emergency call module sends the signal BY PASS to the HU; the emergency call module provides diagnostic methods for HU and emergency calls. Whether the MIC connection between modules is normal;

1. Is the MIC IN connected to the TLV320AIC3104-Q1 and able to supply the MIC Bias (8V, 10mA) sufficient? And can it detect whether the MIC is normal (Open, short GND or power)?
2. Can the MIC IN be connected to the TLV320AIC3104-Q1 and be able to BYPASS the MIC IN to the MIC OUT to the host MIC? Or do I need to plug in an external audio analog switch (SPDT Analog Switches)? If an external plug-in is needed, please suggest the vehicle specification number.
3. Does the LINE OUT output have a self-test function?
Many Thanks,
Jimmy