Hi,
I am new to audio engineering and struggling with audio capture using screw terminals.
I have a TLV320AIC3104EVM-K board set up with the EVM GUI. Using 3.5mm jacks I am able to capture and listen to audio on different headsets using the following commands:
w 30 01 80 w 30 07 80 w 30 19 80 w 30 08 20 w 30 25 E0 w 30 26 10 w 30 2E 80 w 30 3F 80 w 30 41 0D w 30 33 0D w 30 0F 2B w 30 10 2B
I am currently trying to wire an aviation grade headset onto the EVM using the 6 wires that correspond to COMM L, COMM R, MIC HI, MIC LO, VIN and GND. Connecting GND, COMM L and COMM R to the positive HPLOUT and HPROUT terminals respectively provides audio.
What I am unable to get working is wiring the MIC HI and MIC LO pins to a terminal that produces output.
All jumpers are set in their default positions.
The microphone has a bias operating range of 8-16VDC which I have attempted to supply via the voltage wire from the headset.
What typically happens is straight noise with no audio capture, or the on-board microphone takes over.
Any advice on what terminals to use and commands would be very helpful.
Thank you.