Part Number: OPA1656
Other Parts Discussed in Thread: LM3886

Hello, i want to ask a question about the OPA1656.
I connected the component as shown in the figure (both channels), supplying them with ±15V.
The component must replicate the input signal without a gain but giving it more current capabilities, since it have to pass througth a 33R resistor (60 mA max).

The result is saisfying (the green signal is the input, and the orange and yellow ones are the output. The blue is the calculated current. The image shows a trianguar wave but the results is perfect also with all other waveforms.
Now the problem: the component becomes very hot (over 120°C or 248°F when i turned off everything but it was still increasing) during run and stay at around 92°C or 200°F when supplied but not working).
I also noticed that lowering the supply voltage to ±5V dramatically reduce the heat (60°C or 135°F) in running condition, around 35°C or 95°F in only-supplied condition.
Is this normal? Did I do something wrong? Any help will be appreciated.