This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424E-Q1: About automatically retrying DC diagnostics

Part Number: TAS6424E-Q1

Hello everyone,

We are planning to use the function that automatically repeats DC diag in our product.
This is based on the method described in sloa286's application report.

Page9
>If the DC diagnostics are triggered automatically before entering MUTE or PLAY mode, the device will keep retrying without a control command being needed if any fault is detected.

When I monitored the waveform, it appeared to be repeating at a 1000ms cycle.

I would like to know how much this cycle time changes depending on the parts (or surrounding circuit design).

Are there any detailed explanations or application notes about the features?

Thanks,Miyuki