Hello, I'm Jeon Hyeon Min
Although I read DRV2700EVM-HV500 User's guide so many time, I don't understand how to use DRV2700EVM-HV500.
Here's my questions.
1. I'm using piezoelectric actuator which has 0.8 uF. When I connect actuator to DRV2700EVM-HV500, 100Hz output looks strange. See the picture below
SW3, SW4 are stay up to limit 158V, analog input to TP1 and ground to GND, computer is connected to DRV2700EVM-HV500 using USB.
Is there any wrong in setting?


2. When I insert USB to computer to supply 5V to DRV2700EVM-HV500, I can see 158V DC output through oscilloscope. Load is an capacitor which has 0.33uF. Output voltage is shown in the picture below.

Next, I connect function generator to TP1 and GND, turn on function generator(0~3V, 1Hz) and the result is shown in the picture below.

Is the response normal?
I don't understand DRV2700EVM-HV500's mechanism.
In User's guide(picture below), 0~3.3V 100Hz sine function analog input is blue graph and capacitor load is 22nF. so the result is green graph right?

What should I do to see that clean green graph?