Part Number: TAS5806MD
Other Parts Discussed in Thread: TAS5806M
Hi, TI support team
I have received inquiry from customer.
1. Can TAS5806MD use the DSP Memory Register below?
Do I need an external storage device such as eeprom or flash memory to use it?
2. If the DSP Memory is built into the TAS5806MD and can be used without a separate external storage device, how can the DSP Memory Register be used?
Signal interface is I2S.
Can I write in the following order: Slave address + Sub address + Page Value + Value?
3. Is the default value of the DSP Memory map of TAS5806MD the same as the Default value of the DSP Memory map listed in Doc "TAS5806M_ Process Flows.pdf"?
(The number of registers is too large, so we will only process the code with changes)
Thanks.
Regards,
MJ