Dear,
Customer have some question after test, the test result shows as word attachment.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
Customer have some question after test, the test result shows as word attachment.
hi,
usually for audio circuit, we only consider the signal <20kHz for human ear cannot hear signal over 20kHz.
usually, we test THD use AES17(20kHz) which filter out the signal over 20kHz.
no need to use the other filter to filter the AC harmonics at 450kHz.
it would be better to use Audio Precision to test the THD for your output to see whether any problem exist.
tks
jesse
Hi
About your questions:
Question 1: If the nominal harmonic index needs to be reached, additional filtering circuit is needed to filter the AC harmonics of 450kHz/900mVpp.
Yes, the results tested in the datasheet use the AP's filter. The purpose is to filter out the harmonic more than 20kHz.
Question 2: I If a filter circuit is really needed, is there a reasonable filter circuit recommended for resistive loads (such as increasing inductance for T-type filtering, or multistage LC filtering)?
You can take below links as a reference.
AUX-0025 / 0040 / 0100 Switching Amplifier Measurement Filters - Audio Precision (ap.com)
We recommend using AP to do the test.
BR.
Wei Qiu.