Part Number: SRC4184
Hello,Team,
I have questions about SRC4184IPAGT and CDCE913PW
・SRC4184IPAGT
Q1
Are there any AC Operating Conditions which is related with RCKI,
for example, setup,hold and synchronization with BCKI/O,LRCKI/O,TDMIand so on.
Q2
According to Figure17 in datasheet,i can see RCKI signal are inputed to each devices(SRC4184)which is controlled in slave mode from 1 clock generator which devide the line to 3 lines.
Should i devide clock signal from 1 clock generator? I mean, should i use RCKI to each devices in sysnc?
for example, in case using CDCE913PW for clock generator,CDCE913PW output CLK which is made from the same Pdiv1 and connect such as "Y1-SRC1/Y2-SRC2/Y3-SRC3",are there any problems?
・CDCE913PW
Q1
Is there any latency between Y1 to Y2/Y3, when this devide is set to use Y1,Y2,Y3 from Pdiv1?
Q2
Why is there difference about M,N,freq for PLL,in Clock Pro between when using only Y1 and when using Y1/Y2/Y3,in spite of using the same Inclock and the same out Freq setting.
I guess there is no change to set Y2/Y3 to use from Pdiv1 which is used for Y1 setting.
Anyway, in this case that this device to use Y1/Y2/Y3 the same freq and the same Pdiv,i can use reg setting refer to BitViewer in Clock Pro,is that OK?
Q3
In Clock Pro, why i cannot see reg15 nad 31 in BitViewer?
Q4
If i set reg"EEWRITE" to 1 for save the data to memory, is reg"EELOCK" set to 1 immediately without operating reg"EELOCK" setting?
Thank you for your support