Hello,
Currently using a TPA3255 board to drive a 12 inch coil (80 turn 3mH .65 ohm DC resistance). What is the maximum coil inductance that the TPA3255 can drive?
If I use a larger coil, will it damage the TPA3255 or cause heating / reduced power?
I would like to match the datasheet speaker impedance of 2-4 ohms but am concerned about possible damage from higher inductance.
Any guidance would be helpful as the TPA3255 has performed well for us.
Thank you
Chris