Other Parts Discussed in Thread: PCM5121, TAS5825M, TAS5805M
Hi,
We are using TPA3130D2DAP in our design with 15V supply. We are using MCU 3.3V logic and we would like to control TPA3130 via 3.3V MCU IOs. Please answer the following to clarify;
1. I can see FAULTZ is open drain so we will add a pullup to 3.3V along with shorting it to the SDZ Pin. As per SDZ its TTL logic levels with compliance to AVCC. We will be using 15V to AVCC but as per recommended operating conditions SDZ pin VIN min is 2V so can you please confirm if we are good to go with connecting it to a 3.3V IO from the MCU?
2. Please confirm if same applied to MUTE pin by controlling it via 3.3V IO?
3. Can we control the volume for the audio amp via GAIN/SLV from 3.3V MCU IO? As per TPA3130 Eval board the design has pull-up at GAIN/SLV pin connected to the GVDD pin, same as per datasheet. Please note that we are using PCM5121PWR as Audio DAC before TP3130 so can we control the volume of PCM5121PWR instead of doing it for TPA3130? As per PCM5121PWR data we have Digital Volume control so I am assuming it will be done via I2C. Please confirm
Thanks