This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC5140: AGND and DGND

Part Number: TLV320ADC5140

Hi team,

Looking at the connection example described in the specification, the GND of ADC5140 is connected only to the AGND (the ▼ mark in the figure below).

DGND is connected to the DREG and IOVDD through a bypass capacitor.

Although the AGND and DGND of the customer schematic are separated, is it desirable to connect the AGND and DGND at a single point close to the the chip? Or is it better not to separate?

This is because the noise superposition via GND originating from the I2S line with the master device is an issue, and it is assumed that this IC is caused by a small potential difference between analogue ground and digital ground at the digital ground.

Could you please tell us about the GND routing?

Best regards,

Hayashi