Hello,
I have a question about Power on Sequence. of "TPA6139A2PWR".
In my circuit, 3.3V is applied to "MUTE" pin, while VDD is "Low".
Is the MUTE pin tolerance?
Is this harmful to "TPA6139A2PWR"?
Best regards,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yana,
Enabling MUTE before VDD power up is not the recommended sequence, this may increase the possibility of pop noise as described in data sheet section 9.4.2
In addition to that, this device specifies that MUTE pin abs max is VDD+0.3V, so if VDD = 0V this would take the device out of specified conditions.
In cases like this, there's risk of damaging the internal diodes. If VDD=0 and being reversed biased through MUTE pin, the VDD supply connection is made through internal circuitry, if device is enabled and there's input signal, all the current required for the operation would flow through this internal circuitry from MUTE to VDD.
Best regards,
-Ivan Salazar
Applications Engineer