I want to use the DIR9001 to decode the HDMI ARC signal from a HDMI connection. As far as I understand it, that signal is basically a S/PDIF signal with a different amplitude and termination resistance.
The problem is that I do not know how to connect the HEAC+ line to the DIR9001 for single mode transmission. I used the DIR9001 evaluation board as a reference to design the following schematic (thinking it would be similar to a COAX signal), but the TV I connect to seems to only start the ARC transmission when R12 is removed. Why is this, and is there a better way to connect the two together?