Part Number: PUREPATHCONSOLE
PUREPATHCONSOLE is only available for Windows and Mac, but I run Debian. I successfully installed it with Wine (9.0) but it won't run.
[32:0221/013016:ERROR:network_change_notifier_win.cc(157)] WSALookupServiceBegin failed with: 8 [32:0221/013017:ERROR:gpu_process_transport_factory.cc(418)] Failed to establish GPU channel. [32:0221/013020:ERROR:network_change_notifier_win.cc(157)] WSALookupServiceBegin failed with: 8 [32:0221/013020:FATAL:render_process_host_impl.cc(479)] Check failed: !g_exited_main_message_loop. wine: Unhandled exception 0x80000003 in thread 24 at address 004DF9F0 (thread 0024), starting debugger...
Looking at the installed files, it appears to be NodeJS with node-webkit. It shouldn't be that hard to port to Linux. Many competitors (e.g. ST, Nordic Semi) have native Linux applications. I think TI should too.
But aside from that, has anyone had any success with running PUREPATHCONSOLE on Linux?