Part Number: TAS5825M
Other Parts Discussed in Thread: , PUREPATH-CMBEVM
Dear TI team
We are integrating the amplifier IC TAS5825M into our new products in both BTL and PBTL modes.
We have encountered a peculiar phenomenon when we play sounds integrating low frequency signals with modulated amplitude. It happens when the general volume reaches a certain level.
At first, we were wondering if it was caused by our own electronics but we managed to recreate the same phenomenon on the EVM TAS5825MEVM + PUREPATH-CMBEVM in housekeeping configuration (USB input from PC, 24V DC power supply, 4 ohms load, same as our electronic system). Attached the EVM configuration file, filename “tas5825 config.ppc3”.
It seems that when the sound volume is at fade-in and fade-out phases, and at a certain general level, some faint noise can be heard on top of the amplified original signal. It is not easy to describe this noise, it is like a cracking noise, like if some quantification bits were added or missing. So, it generates some unwanted higher frequency noises, not acceptable especially for our high-end application.
We have generated a dedicated sound file to analyse this issue. Please find it attached “20HZ FS_Fade in_1Sec_Fade Out_1Sec.wav”.
Also attached for TI team to investigate, a recording of the output of the TAS5825M, filename “REC_20HZ FS_Fade In_1sec_Fade out_1Sec.wav”.
To ease the understanding of that issue, we have made a 50Hz high pass filtering of this file, attached as “REC_20HZ FS_Fade In_1sec_Fade out_1Sec_HP filter 50Hz 48db.wav”. One can hear clearly that there is unwanted noise at fade-in and fade-out phases, but not during constant volume phase. And one will notice that this effect is not random, it follows the input sound wave with the same pattern all the time.
We would be very grateful if you could help us understanding the root cause of this issue.
Many thanks for your support.
Best regards,
Stéphane.tas5825 config.rar