Part Number: DIT4096
Other Parts Discussed in Thread: DIR9001
Hi All,
I have a question regarding DIT4096.
Please tell me the delay time from input to output.
Best Regards,
Ishiwata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ishiwata,
There is no specific data for this part, the only piece of information that we have is from a pervious post that it suggests:
The data sheet states that the DIR9001 delay from SPDIF input to LRCKO toggle is 3/Fs, meaning at 48 kHz sampling, will be 62.5 us, and less at 96 kHz. I do not have a measurement for the DIT4096, but I do not think it would be too far off what the DIR's delay is.
Regards,
Arash
Hi Arash、
Thank you for your answer.
I have an additional question.
I plan to use multiple DIT4096.
If the input timing of each device is the same, will the output timing be different?
How many Fs will change? Or does it shift?
I don't think the output timing of each device is significantly different.
Best Regards,
Ishiwata
Hi Ishiwata, You are most welcome.
Delay is sampling frequency dependent, so they all would propagate the same with 3/Fs delay( as we established from above) .
Regards,
Arash