Part Number: TLV320DAC3100EVM-U
Other Parts Discussed in Thread: TLV320DAC3100, TLV320AIC3100
Hi,
we have connected TLV320DAC3100 based ACEV-1A EVM to imx8Mini eval board.
we are able to operate the 8ohms speaker and detect 3.5mm jack headphone insertion also on ACEV-1A EVM .
we would like to know
1)if TLV320DAC3100 would detect mic analog input (when user is speaking on the microphone of 3.5mm jack headphone cable) and provide it to the imx8mini processor using BLCK/MCLK/DIN/DOUT?
2)if point 1 is true then how would it be possible in firmware
3)if point 1 is false then how can we process the mic analog input from 3.5mm jack and interface to processor