I want to use codec in differential input and output mode. Do I need to use both left and right channels or either Left or right channel can be used for giving differential input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use codec in differential input and output mode. Do I need to use both left and right channels or either Left or right channel can be used for giving differential input?
Hi Vinay,
Yes to use differentially you need to use both inputs. See the picture below. You need to use both IN1_L and IN1_R to create a differential pair.
Best regards,
Jeff McPherson