Other Parts Discussed in Thread: LM4670
Hi TIer
I think I meet a same problem with e2e link:
When I try to go to the maximum volume, I find that there is no output on the chip's speaker output. I checked the registers and found that the HPL shows the short circuit protection status. I removed the capacitor from the LC filter as in the previous E2E link and the circuit resumed. So I'm thinking about the root cause of the LC L = 33uH C = 10uF filter design error?
1. Also, for some reason, customers have added a first stage D class amplifier LM4670 in between the LC filter and the 9 ohm horn and set it to a gain of 1 .


2. Does this cause the TLV320 load impedance to become large and may increase the oscillation of the LC, which causes short-circuit protection?
3. I captured the waveform on the positive and negative output of the speaker to ground when the short circuit protection occurs. It doesn't look like overshoot is happening .

4. The audio signal of the sound is around 650 Hz and I checked the LC capacitor PN: MSASG32NSB5106MTN.
Could you help me determine the root cause, thank you.