Part Number: PCM1821
Other Parts Discussed in Thread: TLV320ADC3120
I need help choosing an ADC for my device. It is a electronic stethoscope for heart and lung auscultation. From literature review, heart sounds are between 100-200 Hz and lung sounds around 2000 Hz, and the best method is a condenser microphone. So I would like an adc to pair to this microphone, outputting I2S which will be sent to an ESP32 chip. I will only be using one microphone. If there is an option to offload some of the filtering from the ESP32 to the ADC that is ideal but is not required. Do you have any product suggestions?