Dear Expert:
We connected a simulated MIC at pins 1 and 2, as shown in the following figure,
In a stationary state, i.e. without external sound sources, the waveforms of BCLK_ADC, FSYNC_ADC, and SDOUT_ADC are measured as follows: the blue signal is BCLK_ADC, the yellow signal is FSYNC_ADC, and the green signal is SDOUT_ADC。
After zooming in on the red box, as shown in the following figure:
My question is, why does SDOUT_ADC have output without a sound source?
We grounded the input terminals, MIC_ANA+and MIC_ANA -, and still saw data output in SDOUT_ADC, but it is unclear where the problem lies.