Part Number: PCM5242
I want to use a PCM5242 DAC. For normal operation at various sample rates I want to use the default program 1 which is a interpolation filter that can be configured to allow x8/x4/x2/x1 oversampling for the DAC. According to table 7 (ROM Preset Programs) in the datasheet, the DSP needs 256 cycles for this filter per sample, which means, the DSP frequency has to be at least 256 times the sample frequency.
According to the datasheet, for 192 kHz a 2x oversampling is used internally (which means I need an interpolation filter).
The first line in the table shows this case. I understand where the prescalers for the OSRCLK and the DACCLK (NDAC and DOSR) come from. However, I don't understand, how the DSP frequency is calculated. The table lists a DSP Frequency of 24.576 MHz (=SCK), which is only 128 times the sampling frequency. So according to table 7 (see above), this is not enough to run the interpolation filter.
I know, that I can simply configure the PLL in the PCM5242 and generate a 256 times 192 kHz clock solely for the DSP which essentially is still in range of the clock spec. and would work as far as I see.
However, the datasheet explicitly lists the lower DSP frequency. How is this possible? Do I need to write a custom program for the DSP in that case? (Which I want to avoid because I simply want a DAC).
In 384 kHz Operation the case is similar. No matter how the device is clocked, the DSP will at most run at 49.152 MHz (128 times the sampling frequency) which is too low for the interpolation program. I'm aware, that I don't need an interpolation filter for 384 kHz operation, since the oversampling is x1. However, the DSP program cannot be disabled, as far as I see. A program is always active.
How to use the DAC with this sample frequency?