hello,
We are not familiar with the device TLV320AIC3204 and have a problem:
The hardware drew a Demo board according to Section 10.2 "Typical Application" in "TLV320AIC3204", as shown below:


The three-pin MIC is connected to MICBIAS, IN1L, and GND
The headset is connected to HPL and GND
Question now: Is the hardware design wrong? How to determine whether the 3204 is working properly? How do you determine if the register setting was successful?
Try to give LDO_IN for 3V3, external IC for MCLK, WCLK, BCLK, SCL, SDA, send register configuration through I2C, no response. Again to LDO_SELECT and IOVDD for 3V3, still no response. SCL and SDA were raised with 4.7K, but there was still no reaction.
Both device addresses 0x30 and 0x18 sent by I2C have been tried
The register configuration sent is