Other Parts Discussed in Thread: PCM5242, TAD5142, TAD5112
Hello
I'm currently developing a new DAC circuit for our audio amplifiers as the old DAC is obsolete.
We've been trying out different ICs to handle the conversion, and the PCM5252 seems like the perfect candidate.
I've designed a prototype board and used the LT3042 LDO @ 3.3V as a power supply. I've followed some example circuits and got the DAC working in Hardware Mode.
The issue I currently have is, when the I2S data is enabled but the generated sine wave is at -150dBV or lower, I have a noise floor of -99dBV, which is about 12uVrms.
When the I2S is disabled or the Soft mute function is enabled, the output noise floor drops to about -115dB, which is the lowest my audio analyser (Quantasylum QA403) can get. So this means the muting function is working as intended.
However, when playing a 1kHz Sine @ 2Vrms, the measured SNR of 99dBv is much lower than the 114dB described in the data sheet.
Does someone have any idea what the origin/source of the noise could be? I've tried using both LT3042 LDO en MIC5202-3.3 but this didn't change anything noise wise.
Any help is much appreciated!
Kind regards
Simone Matthys