Part Number: OPA1655
Other Parts Discussed in Thread: TINA-TI, , JFE150EVM
Hello team,
Using the OPA1655 under dual supply conditions (VS = ± 3V) to amplify a 10 kHz square wave modulated signal. The closed-loop bandwidth (or cutoff frequency) of the OPA1655 system I have designed is ~100 kHz. The simulated output noise density I simulated with TINA-TI and corroborated with hand calculations at 10 kHz is 3.73 μV/√Hz and I would like to try and keep it as close top this value as best as I can... which brings me to this discussion regarding power supply noise and bypass/decoupling capacitors.
I am using a B&K 1760A DC Power Supply which is rated to have a ≤1 mV rms ripple (assuming 20 MHz bandwidth as it is not specified in the datasheet attached). Neglecting 1/f flicker noise, the equivalent output noise density of this power supply would be 2.2 μV/√Hz broadband. I would like to reduce (or eliminate if possible) this power supply noise to be 3x lower than the 3.73 μV/√Hz from my OPA1655 output noise at 10 kHz.
I plan on using 100 nF NP0/C0G package capacitor (for low ESR) as bypass capacitors and a 4 layer PCB with ground/power planes as suggested in Section 8.4.1 of the OPA1655 datasheet.
If I want to further ensure good signal fidelity and reduce power supply noise should I:
1. Use additional low ESR ceramic and/or electrolytic caps in parallel to the 100 nF ones such that the equivalent low impedance if the capacitances span the GBW of the OPA1655 or only the 100 kHz BW of the OPA1655 system I designed? (worried to use more capacitors due to possible resonances.)
2. Use ferrite beads instead of additional bypass capacitors?
3. Is a capacitance multiplier circuit such as a emitter-follower NPN RC filter (referring to this video https://www.youtube.com/watch?v=wopmEyZKnYo) better to remove power supply noise compare to options 1. and 2. ?
Any other suggestions are welcomed and appreciated!
Thanks for taking the time to read my post! (Apologies if any of these questions are mundane, it is my first time designing an analog circuit let alone a high precision/low noise one...)