This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3251: After dumping the current state into a header file, the DRC function cannot function properly.

Part Number: TAS3251

Hi TI team:

Debug the DRC function using TAS3251EVM, and DRC can work normally on the EVM board.

After dumping the current state into a header file, the DRC function cannot function properly.

Some settings do not match the actual parameters set, such as the DAC gain setting of 7.5dB, but the exported file does not reflect this value. Does this gain need to be manually adjusted?

This problem has occurred. Is there an error in the settings? Can you provide the correct operating method?

Is the PPC3 file in the attachment and the exported. h file correct?

   TAS3251_DRC.zip