Other Parts Discussed in Thread: TPS61089, TAS2781, LM5155EVM-BST, , LM5155
Hello,
I have been having issues getting the EVM to output a portion of the rated power into 4Ω at 1%. Figure 6-4 and 6-5 of the datasheet lead me to believe that I should have no issue hitting 10W into 4Ω.
With the TAS2781 and integrated TPS61089 I am only able to get around 6W before significant clipping occurs. The PVDDH rail does reach up to ~12V at this time, but I start to see PVDDH fluctuate and the FB pin drops below the FB voltage.
Because of this I switched over to a LM5155EVM-BST that is more than capable of the 10W required. After struggling to get the Class H configuration to work properly between the TAS2781EVM and LM5155EVM I resorted to fixing the LM5155EVM-BST output voltage to ~12V and then ~13V. At 13V I am still seeing ~2.3% THD at 10W and -4dBFS. I am using 12AWG jumpers and only see the rail drop to 12.998V at C8/C9. The distortion is also asymmetric with clipping only happening on the negative side of the waveform with the current voltage rail.
I have added in a 15uH inductor in series with the positive side of the resistive load. I believe this should be inline with the datasheet.
I will continue to boost the voltage rail via a bench supply and see if I can hit the target distortion at a high rail voltage.
Do you have any possible ideas why the EVM would not be hitting 10W with a 12V input on PVDDH?
-Adam