Part Number: MC33078
Hi'
Could you please help confirm whether the output port of the op amp is equipped with TVS
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MC33078
Hi'
Could you please help confirm whether the output port of the op amp is equipped with TVS
Thank you
Hi Yingjiao,
MC33078 has internal ESD protection diodes on the outputs but these are not TVS diodes. Please see our video series on overstress protection for more information on external protection methods like TVS diodes: https://ti.com/video/4080379002001
Is there a reason there is a concern for the output protection for the MC33078?
Regards,
Ashley
Hi
What about input port protection?
The input port has a clamp diode to the power rail
Hi Yingjiao,
Is this clamp on both of the inputs? Could you provide a schematic visual to show what you mean.
And also, could you clarify what performance problems you are seeing with the MC33078?
Thanks!
Regards,
Ashley
Hi Ashley
We have described the corresponding problems in the following pictures, please help to confirm
thank you


.


Hi Yingjiao,
Could you show what is on the output of U2A and U2B? When is the Vin waveforms during the power on sequence? During the first brief VCC increase?
Regards,
Ashley
As shown in the figure,ch1 refers to In1+,ch2 refers to In1-,ch3 refers to In2+,ch4 refers to In2- of U2 during the power on sequence。

Hi Hongyao,
To clarify, I am asking for the output pin waveform here:

Also what is U1?
Regards,
Ashley
Hi Hongyao,
Thank you for the additional information.
It is recommended to add a resistor here so that the current limit is not exceeded for the absolute max. The positive input pin can be connected to ground, but it is recommended to also add a resistor to prevent ground bouncing issues and reduce offset error.

The current waveform showing the differential input would not damage the part. Having the short VCC increase before power on should not damage the part as long as the input currents and input voltages do not exceed absolute maximum spec.
Please let me know if you have any questions.
Thank you!
Regards,
Ashley
Hi Ashley,
Thanks for your replying. I have no other questions temporarily.
Thank you!
Regards,
Hongyao Liu