Part Number: LM833
I am inputting ±15V to the power supply, but it broke down due to a phenomenon in which the resistance value between the power supplies became low.
There was no problem with the peripheral circuits, only the IC was broken.
I tried introducing noise (period: 16ms, pulse width: 1us, amplitude: 100V to 4.1kV, -100V to -4.1kV) into the power supply line, but nothing failed in the same way.
What could be the cause of the failure?
(Sorry if this is the wrong forum to ask this question)