Other Parts Discussed in Thread: PCM1780
The composition of the whole link is: audio input -- > PCM1862 (ADC) -- >PCM1780(DAC) -- > Audio output; However, in the case of high frequency, the output audio amplitude will be reduced, and the waveform is relatively complete (see the pic1-1k5 input, pic2-4k input). The input and output points of the test are the direct-connected input of adc and the direct-connected output of dac, and there are no other OPA
See pic PCM1862,pic PCM1780 for the register configuration of PCM1862 and PCM1780. The default value is the register that is not configured.
pic1-1k5:

pic2-4k:

pic PCM1862:

pic PCM1780: