Part Number: TLV320ADC6140
Other Parts Discussed in Thread: AM5728, , PCM5122, ADS8361, TAD5212, TAC5212, TAA5212
Tool/software:
For my application, I am using an AM5728 running Linux and want 2+ch audio at 16 bits in and out at a non-standard rate of, for example, 240kHz. I also want to use TDM/DSP mode over McASP for ease of integration into Linux. I'm not interested in using any of the extra features like programmable filters or AGC, I just need samples in and out. These will be driven by an external reference with one converter operating in Master mode.
My questions are,
- Does the TLV320ADC6140 support non-standard rates? For example if I supply and external clock of 15.36MHz (or 30.72MHz) could I configure the device produce 2*16bit streams at 240k in either Master or Slave mode?
- I'm aware of the 80kHz signal bandwidth limitation.
- I've requested PurePath 3 and perhaps my answer is in there based on section 8.3.2 of SBAS992A
- The same as #1 but using a PCM5122 DAC. Documentation for this device seems to indicates this is completely possible.
If this is not possible with both, are there active production TI offerings that I can use that both support TDM/DSP mode? I've located precision ADCs like the ADS8361 that support TDM, but no DACs.
My goal is to have a 2-channel ADC/DAC pair, either as an integrated CODEC or separate IC's, that can operate with TDM/DSP at non-standard audio rates near 240kHz with 16+bits and are configurable over I2C. I have the option to use a single or separate McASP ports, so a CODEC or separate IC's are both options.
Thanks in advance,
Jacob