Part Number: TAS2781EVM
Other Parts Discussed in Thread: TAS2781, TAS2780, TAS6584-Q1, TAS6422-Q1
Tool/software:
Hi,
I am trying to configure the TAS2781EVM to generate the maximum current output that it can continuously across a 2ohm resistor.
From the datasheet the protection circuitry indicates the minimum current under "Output Over Current Limit on PVDDH" is 5Apeak ~=3Arms. I assume that the output is capable to source this current magnitude.
At this moment the highest rms current that I can source the the EVM at ROM mode only, with every protection setting removed is <1.5Arms continuously. I have played around the ppc3 device control panel and wasn't able to operate the evm close to atleast 2.5Arms without the ppc3 throwing IR fault of overcurrent. I have also tried supplying a 12V 4A supply to PVVDH and use the PWR_mode0 and didn't make any improvement.
At some point the evm behave with lower current with similar setting for some reason with all the thermal and BOP protection disabled.
I also tried ramping the volume slowly to not upset the overcurrent fault with no success..
Could I please request a .ppc3 file that I can use here as a baseline to operate the EVM to max output current continuously @25°C with the load description above?. I prefer all the setting on protection removed as I will enable this myself one at a time accordingly depending on our specification.
rgds,
Jose