This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6140-Q1: comparison with TLV3200adc6140

Part Number: PCM6140-Q1
Other Parts Discussed in Thread: TLV320ADC6140

Tool/software:

This part appears to be very similar (except the package) to theTLV320adc6140.

From a review of the data sheets I see no differences.

Can you tell me what differences there are, if any please?

  • Hi,

    While the PCM6140-Q1 and TLV320ADC6140 have similar performance and features for the most part, there are a few differences:

    • The PCM6140-Q1 is an automotive Audio ADC, whereas the TLV320ADC6140 is not meant for automotive applications.
    • The package is different between the PCM6140-Q1 and TLV320ADC6140, show below

                                                              

                                    PCM6140-Q1                                                                                                                       TLV320ADC6140

    • The PCM6140-Q1 has a “High CMRR Mode” where the device can support higher tolerance on input common-mode. The TLV320ADC6140 does not support this feature.

    Thanks and Regards,

    Lakshmi Narasimhan