Other Parts Discussed in Thread: TAC5242
Tool/software:
TAC5242_EVM is configured as:MD0:GND MD1: 1 MD2: 0 MD3:1 MD4:0 MD5:0
1.MCLK
TAC5242_evm power on and input an analog differential signal waveform test chart.xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
TAC5242_EVM is configured as:MD0:GND MD1: 1 MD2: 0 MD3:1 MD4:0 MD5:0
1.MCLK
TAC5242_evm power on and input an analog differential signal waveform test chart.xlsx
Hi,
Can you explain the issue your facing?
Regards,
Hi,
Try changing your BCLK to be 2.304MHz. At 24 bit depth * 2 Ch * 48kHz Fsync this is the BCLK signal needed.
If you want to have a 3.072MHz BCLK, bit depth should change to 32-bits wide.
Regards,