Part Number: TAS5827
Tool/software:
Hi all,
I have EMI measurements coming up and would like to activate Hybrid Modulation on my TAS5827 amplifier board.
I know that Hybrid Modulation can be activated by setting bits 1-0 in DEVICE_CTRL1 register to 10, but the TAS5827 datasheet states in section 6.4.6.3 that I have to select a process flow in PPC3, which supports Hybrid Modulation. So I'm wondering which process flow is active in the amplifier by default? In case it's "Housekeeping" or "Lite Mode", this would mean that Hybrid Modulation is supported without having to load a full configuration from PPC3.
Second question: is there an easy way to verify if Hybrid Modulation is actually working?
Thank you very much!
Fini