This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
We are using the TLV320AIC3106 Codec in our design, the OS is TI Linux (Linaro tool chain, Arago package) on an AM4378 microprocessor and are trying to configure the specific registers associated with the microphone AGC and dynamic audio compression functionality. Do we need to write custom I2C commands to address these registers specifically, or is access to these registers available through higher level functions? We are using ALSA library to currently manage the CODEC.
Thanks, Pete
Hi,
Yes, you will need to configure through the registers. There's no high-level function from the driver.
Regards.