Part Number: TAS5630B
Other Parts Discussed in Thread: TPA3156D2, TAS5630PHD2EVM, UCC27284
Tool/software:
Hello
While a typical (audio) application doesn't require short propagation delays (and probably that's the reason why it's usually not provided in the data sheets), we want to use a class D amplifier as an AC current source and propagation delay becomes crucial in our application. There are some power stages (with PWM inputs) that do provide propagation delays, but this requires a PWM generator for a relatively high frequency (we would like to use ~1MHz switching frequency). The questions are
1) Are there analog input short propagation delay class D amplifiers working at ~1MHz? (Short propagation delay ~1usec)
2) Are there PWM generators IC with good accuracy (<0.5%) for 1MHz and short propagation delay (~1usec)?
Thanks