This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4392: Using one input only, no output?

Part Number: SRC4392

Tool/software:

Hi,

If I only want to use one input on the SRC4392 is there anything I should do in the hardware design with the un-used inputs?

If I'm not using the output at all is there anything I should do in the hardware design with the un-used output pins?

If mute is only being done through the I2C interface, can I connect the MUTE input pin directly to GND?

Is it ok to tie the I2C address pins (A0 & A1) directly to VIO or GND without resistors?

Thanks,

G