This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULC1001-DRV290XEVM: GUI Error message

Part Number: ULC1001-DRV290XEVM
Other Parts Discussed in Thread: USB2ANY

Tool/software:

Hi Team,

Could you please help this message?

Thank you.

  • Hi Dustin,

    Were you able to successfully update the USB2ANY firmware when that window popped up? You have to use a small pin (like paper clip) to hold the BSL button and update the USB2ANY firmware. Then it should connect.

  • Hi Griffin

    Thanks for your guide.

    I tried to connect, but at some point I got connected.

    However, when cleaning mode is enabled, the current flow is only about 0.3 amps momentarily when the power supply voltage is 12 volts.
    The EVM board says 9~16V, 8A, but I would like to know if it is working properly because less current is flowing than expected

     

     



  • Hi Dustin,

    What lens cover are you using? The new LCS-FL-RNG15?

    Please download the configuration file from Secure Resources - ULC-DESIGN. Also make sure you are using the latest GUI from the same Secure Resources folder.