Other Parts Discussed in Thread: TAS2562
Tool/software:
I have a low power application for the TAS2780, I only need around 1W. Looking at the data sheet, the THD around 1W output is quite low. However the data is measured with VBAT and PVDD powered.
I am considering using PWR_MODE0 and connecting 5V rail to both VBAT and PVDD. According to the data sheet, only PVDD will be used in this case.
This is not a portable application, so I am not worried about efficiency. I just need low THD at low power.
I’m curious if anyone has any measurements of TAS2780 using VBAT=PVDD=5V in PWR_MODE0? Particularly THD into 4 or 8 Ohm loads.
Regards,
Dan
PS. Maybe there are better parts for this application but I also need the ISENSE feature.