Part Number: TLV320DAC3101
Other Parts Discussed in Thread: TAS2505, TLV320AIC3100, TAS2521
Tool/software:
Hello, we're currently looking for an audio codec module which we might purchase in bulk later on. Here is our functional diagram:

Here are the basic requirements for the audio codec:
- Support I2S and stereo output (to drive to speakers)
- Can adjust volume in real time (preferably audio EQ as well)
- Working voltage: about 4v
- Can drive the small speaker (about 1w, 4-ohm). Preferably no external PA needed.
- The chip's start-up time from power-down or standby mode should be small (<4ms), and the quiescent current should be small as well.
We have looked into a few options listed below, and the one that we're most interested in is TLV320DAC3101. I was wondering which one you would recommend the most based on our requirements. I was also curious if there are more solutions besides these that you would recommend.
| TI | TLV320AIC3204 |
| TI | TLV320DAC3101 |
| TI | TLV320AIC3263 |
| TI | TLV320AIC3104 |
Thank you!