This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6584-Q1: Schottky diode recomendation

Part Number: TAS6584-Q1

Tool/software:

The TAS6584-Q1 datasheet recommends that schottky diodes are used when PVDD>14.4V or Fs>480kHz for PBTL.

Does this apply to BTL operation as well?

  • Hi Chris,

    We call out a Diodes Inc. B260A-13-F in the Bill of Material for the EVM.  You basically need a 2A, 60V Schottky Diode.  Look at the spec for the B260A-13-F, and you can use any equivalent.

    At what voltage to you plan to use BTL operation?  If you are above 26Vdc, you should include a Schottky in your Bill of Material. 

    Regards,
    Gregg Scott