This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3204 beep generator problem

Hello everybody!

We have problems with the beep generator example of aic3204. Thats the example I found in another thread (last post of thread from J Arbona).

I had to adapt the code so it fits our requirements. You can find our initialization array below.

We are using the spi interface. Writing to and reading registers back works, so spi interface might not be the problem.

Some additional information:

- Ref pin after initialization = 0,9V

- 16MHz osc

Unfortunately I can not hear any signal.

Maybe you can find any fault in the initialization array.

Best Regards,

Oliver

 

unsigned int beep_array[52] = {
// RESET
    0x0000,    // Select register page 0
    0x0101,    // soft reset

// CLOCK SETTINGS
    0x0000,    // Select register page 0
    0x0403,    // MCLK -> PLL
    0x0591,
    0x0605,
    0x070E,
    0x08B0,
    0x0B82,
    0x0C87,
    0x0D00,
    0x0E80,
    0x1282,
    0x1387,
    0x1480,

// DIGITAL INTERFACE
    0x1B0C,    // I2S, 16-bit, BCLK and WCLK are outputs
    0x1D00,    // Stereo ADC output is routed to Stereo DAC input

// Configure Processing Blocks
    //Select Page 0
    0x0000,
    //PRB_P25 selected
    0x3C19,
    //Select Page 44, Enable Adaptive filtering for DAC
    0x002c,
    0x0104,

//Configure Power Supplies
    //Select Page 1
    0x0001,
    //AVDD supply
    0x0108,
    //Enable Master Analog Power Control
    0x0201,
    //Set the input power-up time to 3.1ms (for ADC)
    0x4732,
    //Set the REF charging time to 40ms
    0x7b01,

//Playback Setup
    //Select Page 1
    0x0001,
    //De-pop
    0x1425,
    //Route LDAC/RDAC to HPL/HPR
    0x0c08,
    0x0d08,
    //Route LDAC/RDAC to LOL/LOR
    0x0e08,
    0x0f08,
    //Power up HPL/HPR and LOL/LOR drivers
    0x093C,
    //Unmute HPL/HPR driver, 0dB Gain
    0x1000,
    0x1100,
    //Unmute LOL/LOR driver, 0dB Gain
    0x1200,
    0x1300,
    //Select Page 0
    0x0000,
    //DAC => 0dB
    0x4100,
    0x4200,
    //Power up LDAC/RDAC
    0x3fd6,
    //Unmute LDAC/RDAC
    0x4000,
   
//BEEP GENERATOR SETTINGS
    //Select Page 0
    0x0000,
    //Time
    0x4900,
    0x50FF,
    0x51FF,
    //1kHz
    0x4C12,
    0x4D2D,
    0x4E7E,
    0x4FB4,
    //Gain = -40dB, Enabled
    0x4780,
    0x4828
};