Hi
As Title if SPDIF will change the sample rate frome 16K to 48K, CC85xx can convert the sampling rate at TX side or RX side.
Matt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Matt,
The CC85xx supports these four sample rates:
32kHz
40.275 kHz
44.1 kHz
48 kHz
When the sample rate changes the CC85xx master, connected to the SPDIF receiver (audio source), will detect this and change accordingly. This new sampling rate will then be distributed to the other nodes in the network.
-Kristoffer