Tool/software:
Hello,
I'd like to get 4ch DAC output from TAC5112.
Following is desired signal route:
TDM slot 1 -> (DAC1A?) -> OUT1P
TDM slot 2 -> (DAC1B?) -> OUT1M
TDM slot 3 -> (DAC2A?) -> OUT2P
TDM slot 4 -> (DAC2B?) -> OUT2M
I set registers as follows, but OUT1M and OUT2M don't output.
I checked DEV_STS0 value and it was 0xCA, DAC channel 2, 4 were powered down.
Do I need to set any other registers?
Acronym | Address | Value |
PASI_CFG0 | 0x1A | 0x30 |
PASI_RX_CH1_CFG | 0x28 | 0x20 |
PASI_RX_CH2_CFG | 0x29 | 0x21 |
PASI_RX_CH3_CFG | 0x2A | 0x22 |
PASI_RX_CH4_CFG | 0x2B | 0x23 |
OUT1x_CFG0 | 0x64 | 0x24 |
OUT2x_CFG0 | 0x6B | 0x24 |
CH_EN | 0x76 | 0xCF |
TDM settings:
Frame CLK: 48kHz
Word Width: 32bit
BCLK: 128FS(6.144MHz)
Best regards,
N.SAKAMOTO