I have searched and read through the notes on connecting the SGND for the TPA6132A2 stereo amp and do not understand the correct connection.
The doc set specifies SGND as "Amplifier reference voltage. Connect to ground terminal of the headphone". But we have a four layer pcb with the center plane as GND. On any layout we do, the router directly connects the common on the headphone jack to GND and SGND to ground via a via at the closest point to each of these two signals. Therefore they are not directly connected to one another other than by the internal ground plane.
Should we manually run a trace from the common on the headphone jack to an island polygon SGND within the main GND plane and then use this separate ground plane as an isolated ground plane within the inner ground, and finally tie this 'island' ground plan to the main digital ground plane with a single trace? The entire board is digital with the exception of this amp.
Thank you for any suggestions and help.
Robert