Tool/software:
Hello, when I was studying the example register setups for TLV320DAC3101 (section 6.3.10.15 Example Register Setup to Play Digital Data Through DAC and Headphone/Speaker Outputs on the TLV320DAC3101 datasheet), I noticed the PLL is powered up and that a reference clock source (e.g. MCLK) is needed as shown in the screenshot below. I was wondering if this is still required when TLV320DAC3101 operates in slave mode? From what I understand, the codec's clock is provided specifically for generating DAC_fs, but isn't DAC_fs equivalent to the WCLK that my master device already provided?
In addition, the master clock provided by my master device is 1.5238095MHz and WCLK is 16kHz. I was wondering if these values are ok. And could you please provide me with a script for the register settings to support these frequencies?
Thank you,
--Jiahe Liu