Part Number: PCM1681
Tool/software:
Hello,
I am using the PCM1681 in my design with an SCK of 12.28MHz, a BCK of 3.072MHz and a LRCK of 48kHz. I have the 24-bit audio data connected to the DATA1 pin and is provided in Left-Justified format. The DAC is configured to be used with an I2C ctrl interface. I can succesfully communicate with the DAC over I2C, but do not make any changes to the default config. I have verieifed all signals with an oscilloscope and everything looks as expected. However, i do not get any audio on Vout1 or Vout2. What am ìdoing wrong. What might cause this problem?